Sometimes there is a mark on inductors to distinguish direction.
Among Murata products, such marks can be found on the film-type LQP_T series, multilayer-type LQG series and some of the wire wound-type LQH inductors. If the inductor structure is not perfectly symmetric, properties will change with the mounting direction. We therefore leave a mark so that the user will know the inductor has directionality. That way, when they use the inductor, they can hope to make the fullest use of the intended properties.
Figure 1 shows examples of the rate of change in inductance value for different mounting directions.