Select your region & language

InductorsAdvantages of Murata Inductors

Supporting your product development by the technology of Murata. Proposal of the most suitable inductor by extensive lineup.
High Quality and Support     Extensive Lineup          Worldwide Sales and Supply Structure          Development Ability

High Qualith and Support

We are in a generation where high reliability is sought after, such as in hybrid vehicles, electric vehicles and etc., which lead the next generation.
Murata has been taking action to acquire TS, ISO and AEC-Q200 quality standards for on-board electronic components.
We are aggressively moving forward in order to solve the daily issues of customers with our good product analysis technology.
We perform periodic good product analysis, to promote stable quality and improvements in the reliability of products, by information feedback to development.

- Murata's Evaluation and Analysis Technology Provides Security to Customers -

Utilizing state of the art analysis systems, Murata is engaged in "product development", "maintaining of stable reliability" and "improving the reliability of good products".

Murata's Evaluation and Analysis Technology Provides Security to Customers

Extensive Lineup

- Proposal of the total solution only in Murata -

As an inductor manufacturer, Murata provides products for various applications, from power supplies to high-frequency circuits, to meet a wide range of customer needs.

For Power Lines (For Choke, For Voltage Conversion, For Resonance Circuits), RF Inductor (For RF Filter circuits, For RF Choke, For Impedance Matching)

Worldwide Sales and Supply Structure

- Our world wide sales base makes quick responses possible. -

Our sales offices located worldwide allow us to provide our services in a speedy manner.
Murata also has a number of factories worldwide serving as our inductor manufacturing locations. Through these locations, we take steps to mitigate risks such as disaster risk.

Sales Office

Development Ability

- Murata continues to create the future of inductor components, with the development ability making full use of our base technologies. -

Murata continues to make innovations in inductor components towards higher performance, more user-friendly and lower costs, making full use of the 3 base technologies of wire wound, multilayer and film.

Wire Wound Technology Thin copper wire is wound around a core of 0.8 mm in length. Wire Wound Technology Thin copper wire is wound around a core of 0.8 mm in length. Multilayer Technology This is the inner conductor of a multilayer power inductor. It is designed for high power.

- The application technology and material technology support product development, in order to continue creating inductor components suitable for the circuits of customers. -

Based on the catch phrase "everything is to impress the customers and excite the staff", application development in consideration of components expected from the view point of customers, and material development which continues to pursue infinite possibilities, has been supporting the product development.
Murata continues to aggressively challenge the peculiar components required by customers as well.
We will demonstrate our ability to respond, so that customers will think "contact Murata first".

Application Development This is an example of a 3D leakage flux measurement. The leakage is not occurring in the component mounted portion. Material Development The composition and particle size of the ferrite is controlled in consideration of the permeability and internal stress.

- Innovative technology development transforms the innovative components in the creative stage, in pursuit of possibilities into the future. -

Based on applications as the core, the development of Murata's inductor components has expanded using the processes established in other component groups of Murata.

However, under the current conditions, there are areas where we can not respond with this horizontal expansion only.
While understanding the external technology trends, we have established the innovative technology required for the development of Murata's inductor products.

Dreams will expand infinitely, with the technology to form high precision coils, technology to form coils with less resistance, and the technology to realize high efficiency.
Murata will continue to respond to the expectations of customers at a high level, by integrating these technologies with our existing core technologies.

Innovative technology development transforms the innovative components in the creative stage, in pursuit of possibilities into the future.