If piezoelectric film is warped (stretched or contracted) due to pressing force or deformation, an amount of polarization proportionate to the amount of warping in the surface of the piezoelectric film is generated. The charge generated by this polarization is converted into voltage by the I/V converter, and output as an analog signal. The following example illustrates input load and output signal.