Select your region & language

LF Antennas (Antenna Coils)Basic Knowledge of LF RFID

What Is LF RFID?

LF RFID is a form of communication that uses magnetic fields. It is used in smart keys for automobiles and other applications.
When lines of magnetic force pass through a coil, an induced voltage is generated in that coil according to the magnetic flux density.
LF RFID uses this phenomenon to exchange signals.

In addition, magnetic fields are less affected by reflection and diffraction. This means that they create an evenly spaced communication area centered on the transmitter antenna, making it possible to measure the distance between the transmitter and receiver by measuring the strength.

  • Image of Induced voltage e
  • Image of transmitter antenna

Features of LF Communication

1. Measurement of distance with high accuracy

The receiver antenna receives the magnetic field emitted from the transmitter antenna and performs communication in LF RFID. The strength of the magnetic field is proportional to the -3 power of the distance between the transmitter and receiver. Accordingly, it is possible to measure the distance between the transmitter and receiver according to the signal strength.

  • Image 1 of Relationship between the Signal Strength and the Distance
  • Image 2 of Relationship between the Signal Strength and the Distance

Murata Manufacturing introduces a position measurement demo kit so that you can experience the high accuracy of distance measurement with LF RFID.
Please contact us using the Contact Form for details.

2. Battery power saving

It is possible to set the system to active when the receiver antenna receives a magnetic field and to set it to sleep mode at other times with LF RFID. Therefore, it is possible to save power in the receiving equipment.

In addition, LF RFID features lower power consumption in sleep mode compared to other communication methods.

3. Stable communication

LF RFID is a form of communication that uses magnetic fields. Accordingly, it is not affected by human bodies or water, and is less affected by metals than other communication methods, making it possible to measure distances with high reproducibility.

Comparison with other Position Measurement Technologies

LF BLE UWB
Frequency range 30 - 300Khz 2.4GHz 3.1 - 10.6GHz
Distance measurement accuracy

5cm

1m 10 - 15cm
Detection distance

2 - 5m

10m 50m
Impact from interference Low Medium Low
Multipath fading Extremely low High Low
Blind spots None Yes Yes
Power consumption (general)

10mW
15uW (In standby)

50mW
10mW (In standby)
450mW

Role of the Antenna Coil

The antenna coil in LF RFID has the role of transmitting (electricity → magnetic field) and receiving (magnetic field → electricity) the magnetic field.
The transmitter antenna is used as an LC series resonant circuit to efficiently transmit the magnetic field. The receiver antenna is used as an LC parallel resonant circuit to efficiently receive the magnetic field.
Moreover, the receiver antenna has coils wound in three directions to receive the magnetic field in three dimensions.