Select your region & language

Microblower (Air Pump) Application examples

Murata's microblowers are thin and small piezoelectric pumps that feature a high flow rate and silent operation.
We expect these microblowers to be used in various applications including medical and healthcare equipment and general consumer equipment that require downsizing, silent operation, and high pressure.

Medical and healthcare equipment

General consumer equipment

Medical and healthcare equipment

If you intend to use our microblowers in medical equipment, please enter into a separate agreement for medical equipment application before beginning mass production.
Please contact us for details.

  • *All the images used are for illustrative purposes only.

Smartwatches

Murata's microblowers are compact, thin, and lightweight. Therefore, compact design is possible. They contribute to the realization of blood pressure measurement with the oscillometric method in smartwatches. The fit, operability, and design are not impaired even in wearable devices and other compact devices.

Injection pumps

It is also possible to indirectly transport liquids using the air pressure of microblowers. The pulsation of the air discharged is extremely small in microblowers. This realizes air discharge at a stable flow rate. Thanks to this feature, if you use a microblower, you can deliver liquid medicine with little pulsation without directly coming into contact with the liquid even in injection pumps and other liquid supply equipment.

Breast pumps

Microblowers are piezoelectric pumps that suck in air from the suction side and then send that air to the discharge side. It is also possible to use these microblowers in products like breast pumps by using the suction side. Microblowers suck in air by vibrating the piezoelectric element in the ultrasonic band beyond the audible range of humans. Accordingly, you can also use them in environments where operating noise is a concern.

Eye massagers

Microblowers, which exhibit high pressure despite being compact, can also be used in devices with partial pressurization functions such as eye massagers. The amplitude of the piezoelectric elements, the drive source of microblowers, is just a few dozen microns.
You can also use our microblowers in relaxation devices, for which a pleasant feeling is important, without interfering with comfort.

Anti-snoring pillows

In the case of pillows whose height is adjusted by air pressure, such as anti-snoring pillows, the silence of microblowers is useful. The operating sound of microblowers is beyond the audible range. Therefore, it is possible to deliver air without disturbing sleep.

General consumer equipment

  • *All the images used are for illustrative purposes only.

Aroma diffusers

Microblowers have also been adopted in push-type aroma diffusers, which use the power of air to diffuse aroma oils. They can also be installed in portable aroma diffusers because they are compact. In addition, you can adjust the air flow rate. Accordingly, you can also adjust the range of the aroma diffusion.

Gas detectors

You can use microblowers in equipment that sucks in air, such as gas detectors, as well. Microblowers are devices that suck in air from one side (the suction side) and then send that air to the other side (discharge side). Therefore, you can use them in testing equipment like gas detectors as well by using the suction side.

Wine aerators

It is possible to adjust the air flow rate of wine aerators that have adopted microblowers. Accordingly, you can perform optimal aeration to suit each wine brand, even vintage wine brands. Moreover, it is possible to evenly expose the wine to air because you can stably supply air with little pulsation.

Technical Refference