Select your region & language

Timing Devices (Crystal Unit / Ceramic Resonator)High-precision Crystal Units and Thermistors for Automotive UWB
Discrete Configuration and Circuit Design Support

Murata Manufacturing has started offering circuit design support and a discrete configuration that combines the XRCGE55M200MZF1BR0 crystal unit and the NCU03XH103F6SRL thermistor for automotive UWB (Ultra Wide Band).
This product supports automotive applications that use UWB, such as digital keys, CPD (Child Presence Detection), sensors, and Wireless BMS.

Support and cost optimization that only Murata can achieve as a provider of both crystal units and thermistors

Due to the increasing sophistication of digital keys and safety functions, high-precision timing control of broadband communications is required in automotive UWB. However, it was difficult for standalone crystal units to satisfy the required precision in high-temperature environments, and it was generally necessary to compensate with the temperature sensors built into the crystal units.
At the same time, there was a need to use crystal units and external thermistors in a discrete configuration for the purpose of cost structure optimization, but the difficulty of circuit design and temperature compensation posed a challenge. In response, Murata Manufacturing leveraged its strengths in both crystal units and thermistors to begin offering the appropriate part number recommendations and technical support for temperature characteristic compensation. As a result, our solution helps achieve the target characteristics and streamline customer design processes while providing a discrete configuration.

Features of Our Products for Discrete Mounting

Features of the XRCGE55M200MZF1BR0 Crystal Unit

  1. Support for high-precision temperature compensation: Optimizes the temperature characteristic curve in high-temperature environments with our proprietary cutting technology
  2. High reliability for automotive applications: Guaranteed operating temperature of 115°C, low failure rate (particle-free)
  3. Design support: Simplifies design in discrete configurations through our technical assistance for temperature compensation circuits
  4. Stable supply
  5. Lead-free compliant

Features of the NCU03XH103F6SRL Thermistor

  1. Superior solderability and environmental resistance through our proprietary manufacturing methods
  2. Low aging variation and a stable supply
  3. Capable of high-precision support
  4. Supports reflow soldering
  5. The 1005/1608 size series of this product shares the exact same resistance-temperature characteristics, which makes miniaturization easy
  6. Lead-free compliant

Guidelines for Discrete Mounting

When using an external thermistor to compensate for the temperature characteristics of a crystal unit, the crystal unit and thermistor should be placed as close to each other as possible. Refer to here for the general placement position of NTC thermistors. In addition, contact our sales team for case studies regarding the placement of crystal units and external thermistors.

Image of Guidelines for Discrete Mounting

These guidelines were created based on our part numbers that were certified by IC manufacturers. However, these drawings and any related information are valid as of March 2026, and the application notes and recommendations may be subsequently changed by the IC manufacturers.
These guidelines are for reference purposes only. Appropriate evaluations and verifications must be carried out before actual use. Furthermore, the information on this site is subject to change without notice, so be sure to check the latest information before use.

Technical support service examples

Using a crystal unit and thermistor in the Trimension NCJ29D6

  1. 1
    Change the layout of the PCB to facilitate the mounting of the crystal unit and thermistor.
    Reference: Guideline
  2. 2
    After contacting us via the inquiry form, we will provide the shipping address to send the modified PCB to Murata Manufacturing.
    Image of shipping
  3. 3
    Murata Manufacturing will perform a matching evaluation and obtain the TC parameter data to input into the IC/NCJ26D6. We will subsequently provide the results of the matching evaluation and the TC parameter data.
  4. 4
    Replace the TC parameter data on the IC with the Murata data to complete the adjustment.
    Image of replacement

Necessity of Technical Support for Temperature Characteristic Compensation

Risks of compensation with standalone temperature characteristic parameters

The temperature characteristics of a crystal unit are generally compensated using a PLL (Phase-Locked Loop) built into the IC. In a typical design flow, the standalone temperature characteristic parameters provided by the crystal unit manufacturer are written to the IC, and that data is used to perform the compensation. However, the temperature characteristics of a crystal unit after being mounted on a board may not match the individual measurements during testing. The primary cause of this deviation is the change in load capacitance (CL) during board mounting, which impacts the frequency-temperature characteristics.
As a result, there are cases where compensation using only standard parameters may not achieve the optimal precision for the actual environment.

Providing temperature characteristic parameters in the board-mounted state together with matching evaluation services

At Murata Manufacturing, we can measure the actual temperature characteristic parameters in the board-mounted state and provide them as data in the matching evaluation service conducted during the circuit design. This enables high-precision design using the compensation parameters optimized for the mounted board instead of the parameters from the crystal unit's standalone state. Compensation using parameters tailored to the actual mounted device is particularly effective when used in environments with significant temperature fluctuations.