Select your region & language

EMI Suppression Filters (EMC and Noise Suppression)Noise Suppression Product PLT10H (Common Mode Choke Coil)
carnavi

Swipe left or right to change screens View in landscape mode.

Application Examples

Brushless motor power supply units for FA equipment and industrial equipment

For Power Supplies Brushless motor power supply units for FA equipment and industrial equipment

This page introduces problems that often occur with power supply units of brushless motors for FA equipment and industrial electrical equipment, its mechanism, and the solutions.

Noise problems that often occur with power supply units of brushless motors for FA equipment and industrial electrical equipment

The conduction noise from the inverter and power circuit of the motor is too severe!

Large current noises enter when there are lightning strikes! The equipment stops, or malfunctions occur!

Murata's PLT10H solves these problems!

How?

Common mode choke coil in power supply lines of a 10A class which could not be done
with a capacitor only using the PLT10H removes and suppresses noise!

Reasons why PLT10H is effective at noise suppression

  • The PLT10H is very effective at preventing the inflow of noise that occurs in the inverter block, and the noise that flows in from DC input lines.
  • Compared to the common mode choke coils of other companies, the noise suppression of the PLT10H is more effective.
  • This is a hybrid type that suppresses both common mode noise and differential mode noise.

Particularly, the combination shown in the following block diagram is the most effective for noise suppression.

Servo amplifier (controller)

Noise suppression effect of power supply units of brushless motors for FA equipment and industrial electrical equipment

Using the PLT10H effectively suppresses conduction noise from motor power supplies - Example of comparisons with products of other companies -

Noise suppression effect of power supply units of brushless motors for FA equipment and industrial electrical equipment

Inquiries regarding products

Inquiries by e-mail

Click here for consultation and inquiries before purchase

Application Examples