Select your region & language

ESD Protection Devices (anti-static components)Using a TVS diode (ESD protection device) for communication

What is communication?

Communication generally refers to sending and receiving information. Communication can be done over a wire or wirelessly. Examples of each are provided below.
Wired communication: Cable TV, wired LAN, etc.
Wireless communication: Wi-Fi®, Bluetooth®, GPS, GLONASS, etc.

TVS diodes and the issue of ESD with communication

If contact is made with a person or object during communication, this will generate static electricity.
There are many cases where this static electricity travels to an IC and causes a malfunction.
A TVS diode can be used to prevent this issue with static electricity from occurring.

Usage Example

An example is provided below.

Swipe left or right to change screens View in landscape mode
Image of GPS IC/GPS module LXES03TBB1-141 LXES02TAA1-145 LXES03TAA1-199 LXES1UTAA1-157 LXES1UTBB1-157