Radar works by emitting radio waves at a target, receiving the radio waves that return from the target as reflected waves, and measuring information about the target from those reflected waves.
mmWave radar uses FMCW and pulse methods to detect distance, angle, and speed.
The “FM” in FMCW method stands for “Frequency Modulation,” which changes the frequency of the transmission signal over time. A signal with a frequency that increases or decreases over time is called a “chirp signal.” The CW (Continuous Wave) method uses continuous waves and continuously emits radio waves for a set period of time. In this method, the reflected wave, which is the same as the transmitted signal that bounces back from the target, becomes a signal with a frequency that changes over time, which makes it possible to calculate the speed and distance from the target from the frequency difference between the transmitted and reflected waves. Continuous Wave is used in a broader range of applications as a method that can detect speed.
The pulse method emits a short, pulse-like transmission signal and uses the time it takes to receive the reflected waves that bounce back from the target to calculate the distance, etc., to the target. This is a simple detection method that enables a comparatively simple circuit configuration and is often used when high precision is not required.
The following is the typical configuration of an FMCW mmWave radar.
The transmitting side consists of a synthesizer that generates the millimeter wave radio waves to be transmitted and a transmission antenna that emits the transmission waves (chirp signal). The receiving side has a receiving antenna to receive the reflected waves, a mixer that multiplies the received and transmitted waves to create a frequency difference, an A/D (Analog-Digital) converter that converts the mixed signal to a digital signal, and a DSP (Digital Signal Processing) processor, which is a circuit that processes digital signals.
The time required to receive the reflected wave after emitting the transmitted wave varies depending on the distance to the target.
When calculating the frequency difference between the transmitted wave (chirp signal), which has a frequency that increases or decreases over time, and the wave received as the reflected wave, that frequency difference varies based on the distance to the target.
Therefore, when digitizing the IF (Intermediate Frequency) signal formed through mixing and performing a Fourier transform using DSP, that frequency difference is obtained as a frequency spectrum, and the distance information can be calculated from that result.
When receiving the reflected waves after emitting the transmitted waves (chirp signal), a phase difference occurs when comparing the received waves that arrive at multiple receiving antennas. This is because the distance to the target differs between each of the receiving antennas. The angle information can be calculated from this phase difference and the distance differences.
The speed is detected by receiving the reflected waves after emitting the transmitted waves (chirp signal) and using the phase of the IF (Intermediate Frequency) signal formed through mixing. When an object is moving at a speed, the phase differences between the IF signals in the pre- and post-movement chirp signals are due to the time difference before and after the movement, so the time difference of the moving object can be determined from the phase difference, and the speed information can be calculated as a result.