Select your region & language

SensorsSensor Guide Select by Method/Principle

Murata pursued sensing functions making full use of MEMS and processing technology, and magnetoresistive elements including ceramic material technology in order to develop highly efficient and highly reliable devices, modules and systems. A lineup of various sensors respond to the sensing needs of various applications for automobile, wearable, medical care and health care.

Temperature

Thermistors
The resistance changes with the temperature.

Infrared

Pyroelectric infrared sensors
The sensor reacts to the infrared radiation emitted from the human body to output an electric charge.
CO2 sensor
This sensor measures CO2 concentration using infrared light.

Distance

Ultrasonic sensors
The sensor sends and receives ultrasonic waves in order to detect distances from the state of the reflected wave.

Open/Close

Magnetic switches
This switch switches built-in ICs when the magnetoresistive element detects the magnetic proximity.

Inertial force

Accelerometers
This sensor detects the acceleration from the change of the capacitance which occurs in the 3DMEMS element.
Inclinometers
This sensor detects the gravitational acceleration of the Earth to calculate the angle of gradient.
Gyro Sensors
This sensor detects the angular velocity from the change in the capacitance which occurs in the 3DMEMS element.
Shock sensors
This sensor generates an electric charge according to the acceleration (stress) applied to the piezoelectric element.

Magnetic

Magnetic switches
This switch switches built-in ICs when the magnetoresistive element detects magnetism.

Atmospheric pressure

Barometric Pressure Sensor
This sensor accurately measures atmospheric pressure using MEMS capacitance.

Electrical conductivity, moisture water content

Soil sensor
This sensor measures the electrical conductivity, moisture content, and temperature of soil.